Get settings for a system
GET/v1/systems/:systemId/settings
Get the current settings for a system.
The set of settings returned depends on the system generation, indicated by the
systemGeneration field in the response. Only generation 2 systems are supported at
this time.
Some settings are capabilities configured during installation or by the operator; others,
such as storageChargeConstraint and gridExportConstraint, are preferences the end user
selects in the app.
See the individual field descriptions in the response schema below for details on each setting and how they relate.
Request
Responses
- 200
- 400
- 401
- 403
- 404
- 422
- 429
OK
Bad Request
Unauthorized
Forbidden
Not Found
Unprocessable Content
Too Many Requests